Label Assurance

Ensure Compliance through 100% Label Checks

Ensure the Right Product is in the Right Packaging

Undeclared allergen in food product causes detrimental effect on consumers who react adversely. It also leads to costly regulatory non-compliance penalties and loss of market share as consumer trust erodes. Label Assurance by Schneider Electric performs label inspection checks at the packaging line, helping food and beverage manufacturers avoid product recalls due to mislabeling and undeclared allergen.

Simply put, Label Assurance ensures the right product is in the right packaging.

Download the Brochure

How does Label Assurance work?

Watch this video to understand how Label Assurance work to ensure 100% label inspection checks.

Features of Label Assurance

non-destructive

Non-Destructive 100% Label Checks

The inspection camera scans the barcode/data matrix and/or the best-before-date and lot code of every product as it passes through the packaging line. Label Assurance matches the read against the master data for SKU details to ensure the correct labels are used.

This process is non-destructive to the labels and the solution automatically updates the scanned data back to the work order, providing labeling performance status in real-time.

analytics

Pre-defined Standard Reports and Analytics

Quality Engineers and Production Engineers are able to easily perform continuous improvement analytics, saving significant time by not having to research through tons of raw data.

Reports include:
• Production Labeling Summary 
• Work Order / Lot Labeling Summary 

customize

Customizable Conditions

Conditions can be customized to send a trigger signal to the PLC to eject the wrong packaging or to stop the packaging line if the number of non-compliance count is higher than the tolerance count in the time duration set by the operator.

The condition parameters include:
• Number of no read
• Number of illegibility
• Number of mismatch

flexible

Flexible Deployment

Allows for flexible deployment to meet specific needs:

  1. As a standalone quality system:
    • Manual entry of production details
    • Manual start and stop scans
    • Scan data is kept in the solution's database
  2. As part of the MES (integration efforts required):
    • Automated production details integrated from MES
    • Automated start and stop scans with work orders from MES
    • Automated scan data integrated into MES

Discover how a labeling inspection and validation solution can help
Food & Beverage manufacturers avoid costly recalls
Download the Whitepaper

Why Choose Label Assurance?

Solution-based Software

Designed based on established food and beverage industry standards and usage requirements, with standard features incorporated into the software for easier and faster deployment.

The solution is able to link scanned data with work order details for analysis and continuous improvements.

Compatible with Packaging Line

Able to integrate with existing packaging line systems, eliminating the need to set up a separate label scanning station, thereby lowering the cost of deployment. Its highly scalable and secure architecture allows for future expansion.

Partnership with Market-leading OEM
Developed in collaboration with Cognex, a market-leading vison camera OEM, the solution is able to scan and read barcorde/data matrix at high speed, with Optical Character Recognition (OCR) of up to 600 units per minute.
Bundled Services
Experts from the Label Assurance Center of Excellence (CoE) team provide packaged services including consultancy, delivery and knowledge transfer to ensure seamless initial deployment.

Let us tell you more about the solution. Submit your contact details